Small but mighty, the Amazon Dash is a button that you can stick to any surface in your home and then when you run out of something, you just hit that particular button and the item will be reordered for you straight to your door. You set up your Dash Button using the device’s mobile app and then this little gizmo utilises your home’s Wi-Fi network.
There’s no need to be nervous about the kids playing with a button - Amazon uses ‘order protection’ so you don't order products by mistake - you won’t be able to buy the same product until your original order has arrived. You can also cancel items through your Amazon account.
If you are a terrible cook, this futuristic little egg might just be the thing you need. Ask your voice activated Hello Egg for a recipe and it will project videos that show you what to do. This interactive kitchen gadget lets you plan your weekly meals according to your needs, whether that be vegan or vegetarian.
The AI powered device makes it easier for you to stick to a healthy diet and will order your shopping to your door. It also adjusts to unplanned events, like an impromptu meal with a gluten-free friend. Hello Egg is the exciting new kitchen assistant that has been designed to help you and further than that - to think for you.
Do you find it annoying when your fire alarm constantly bleeps to alert you to low battery? When Birdi has a low battery, it will simply order more batteries
This alarm constantly monitors your home’s air quality and takes action. Birdi can detect the difference between burning your dinner where it sounds the alarm but allows you to silence it via your mobile app, or burning material where it sounds the alarm and automatically alerts the fire brigade. Birdi can even alert you when your teenager is smoking a cigarette!
It also multitasks by alerting you and authorities to carbon monoxide, so you can move your family out of the house immediately. This stylish device just may be the most intelligent object you ever put on your kitchen wall.
Buy now for £91
Innovators look to solve everyday problems and this is exactly what Kuvee did when they designed a patented, smart wine bottle which has a valve that prevents oxygen from reaching the wine inside and stops it from spoiling for up to 60 days.
This ingeniously designed bottle allows you to have one or two glasses from a bottle of wine without wasting the entire bottle. The outer material of the bottle is made from recyclable plastic, not traditional glass.
This smart bottle also comes with touch screen to suggest food pairings and tell the history of the wine so that you can impress your guests. The bottles weigh a lot less than a glass bottle, which means about half the cost of normal winery transportation.
For someone who struggles to keep plants alive but loves the idea of home-grown, this is yo ur solution. Impress guests at your dinner parties with your smart kitchen wizardry by using freshly grown herbs using NASA-inspired technology. All you have to do with this magic gadget is add water - that’s it!
Here’s the science - the soil contains a nano-technological growth medium that perfectly balances the water, nutrition and oxygen for optimum growth. All you need to know is that your herbs will grow naturally, without the use of nasty chemicals.
A magic pot seems like something from a fairytale, but this appliance is fast becoming a must-have and has been called a game changer in the kitchen. It already has legions of fans and the reviews on Amazon speak for themselves. Instant Pot is huge on YouTube with large numbers of fans wanting to know the latest tips.
So what makes it so good? The fact is that it does the job of seven or more other appliances: a slow cooker, rice cooker, a pressure cooker, yogurt maker, warmer and deep fryer, saute and steamer food. It can also sterilise, making this the ultimate multitasker.
Freshly baked warm gooey cookies are heavenly, but to bake they take time, recipes, trial and error, washing up, mess - all hassle. That is set to change with the CHiP Smart Cookie Oven which gives you freshly baked cookies in just 10 minutes - with no washing up.
You just put cookie dough in the CHiP oven and choose your cookie texture using the mobile app. You can use your own dough, or the company’s pre-made dough. And because it’s 2017, they also offer pre-made dough in gluten-free, non-GMO, vegan and soy-free variations.
If you like your steak cooked to perfection, you need an Anova Precision Cooker - it takes all the guess work out and all the hassle away.
The Anova clamps onto any of your existing pans and the food cooks underwater in a sealed plastic bag so that the meat is wholly tender. This user-friendly cooker enables you to cook meat with such precision that it is safe to eat, but you will never again overcook meat so that it becomes tough.
The clincher is that is controlled from an app for remote cooking, so you can go about your day while your Michelin quality meal is prepared to exactness.
If you want to boost your 5 a day vegetable intake, the Veggie Bullet is a fun way to do it. The Veggie Bullet offers a 3-in-1 solution, so that you can spiralise, slice and grate. You can spiralise a whole saucepan of courgette in seconds which is so much more economical than buying a tiny tub of courgette spaghetti in Waitrose.
The Veggie Bullet’s beauty is that it is simple to use and it simplifies your life. This kitchen gadget appeals to those who are on a health kick - it makes it easy to prepare a nutritious, home-cooked meal, while saving your precious time.
Being environmentally aware needs to be part of everything we do and the latest kitchen technology is taking this into account. It is a waste heating up a full-size oven just to make one part of a meal.
The Breville Smart Oven is so compact that it sits on your kitchen countertop, yet it functions like high-end appliance. By using it instead of your full size oven you will save on energy costs. It also has an intuitive control panel that makes programming simple. You can adjust its presets and the oven will remember your adjustments for the next time you cook that same item.
For the power of a traditional oven with faster heat times and a smaller footprint in your kitchen, use this stylish Smart Oven.
Not a morning person? Nespresso’s Expert and Milk brings barista-style coffee to your home and allows you to control the machine via an app, so you can make your cup of coffee from your bed. You barely need to move a muscle!
It gets even more impressive - you can create coffee in four different sizes, customise the settings, tweak the temperature, track your pod stocks and order more pods directly. This offers the ultimate convenience for a coffee junkie - it couldn’t be simpler. You can literally wake up and smell the coffee.
You can probably guess from the price that this is no George Foreman. The attraction here is convenience - just throw the meat on the grill and walk away. This is a smart device that can cook your food perfectly with little input from you.
Many of the new advances in latest kitchen technology are geared toward precision and the Cinder Grill is an exact fit. Whatever your choice - duck breast, steak or salmon - all will be juicy and tender with minimal effort.
One of the main benefits of new technology is saving you time and this sleek tap with contemporary Italian design is now essential to any modern kitchen. Waiting for a kettle to boil while you make your hot drink or fill up your saucepan is so passé. It is time wasted, especially if you have guests that you want to get back to.
This stylish tap is also 20% more energy efficient than a kettle, giving you the exact amount of water needed, with no need to re-boil. The handle features a safety locking mechanism so you don't accidentally turn on the boiling water.
Buy the steaming hot water tap for £729
The June Intelligent Oven is basically a computer that cooks. This genius oven identifies your food, weighs it and then cooks it perfectly. It also cooks your food 25% faster than other ovens. Those celebrity chefs should be nervous!
Using the June app, you can control June remotely - just preheat the oven and receive notifications when your food is nearly done. For the ultimate tech geek, it also contains a camera in the oven so you can watch your food cook. We would recommend that you stay within the home while cooking for safety reasons, however tempting it might be to go out.
The Wall Farm is a visionary way to grow fresh vegetables indoors all year round - particularly useful if you live in a city. The smart soil technology utilises NASA technical knowledge and this means that the plants can flourish without any harmful chemicals. The stylish wall display will look trendy in your kitchen and simultaneously meets the current fashion for home-grown.
The Wall Farm uses innovative plant capsules and the capsule starter kits include a choice of four kits - flower, tea, salad or herb. The water tank in the Wall Farm lasts for a month, so remembering to water the plants is a thing of the past. Check out the photos on the Click and Grow website - the displays look fantastic.
This leading dishwasher shows off the latest technology. As with many items in a smart kitchen, it has an app where you can remotely check wash cycles and download personalised wash cycles. If there is a problem with your dishwasher you can get immediate help through your smartphone.
With four spray arms instead of the usual two, it cleans your plates, cups and glasses from all angles and saves about 5,000 gallons of water every year. You can set two different intensities for water spray, which means you can power wash pots and pans and delicate wash glasses in the same load. It is also quieter when in use - all adding to the beauty of this streamlined interactive kitchen appliance.
The LG Smart Washing Machine has a Centrum suspension system, which uses shock absorbers to soak up vibrations during heavy wash loads and spinning. This means no more damage to your machine, which means that it will last longer.If you live in a flat it will also mean that you no longer annoy your neighbours or damage your floor or ceiling.
This high-tech machine also ingeniously uses steam to remove 99.9% of allergens for an ultra clean. The drum holds a huge 12kgs and the Turbo Wash function powers through a load in an amazing 49 minutes so that your laundry doesn’t pile up. Finally, you can of course operate the wash remotely using your smartphone - so you can simultaneously do a wash while you are out and about.
Want to speak to a member of our team? We’re here to help