Parenthood is a wonderfully rewarding experience yet at the same time it is often worrisome, especially for new mothers. Taking home your precious newborn leads to a whole new world and nothing will ever be the same again! While you may well be equipped with all the right products to cope with looking after your newborn there are always those extra items that go a long way to making life easier.


Look for time-saving Gadgets


As a new mum, much of your time will be spent in the kitchen, whether preparing bottles for your baby, sterilising used bottles, washing up or doing the laundry. Those first few months are exceptionally busy and usually centred around feeding times and getting your baby into a suitable routine.

It’s at times like these that you need good quality kitchen equipment to help make life easier, more convenient and save you time. Time is extremely valuable and often the days run away because they’re so busy.

It’s always useful to have a couple of extra gadgets to make life smoother and free-up some of that time so you get a well-earned break! With InSinkErator there are some fantastically useful appliances designed to make life so much easier. These gadgets stretch beyond babies and toddlers too so they’ll be used throughout your child’s early years and be a part of everyday family life for many years to come.





Look for time-saving Gadgets


Hot Water on Demand


An InSinkErator instant hot water tap is one of those gadgets that every home should have because of its convenience and flexibility. When you’re a new mum, time is of the essence especially if you’re trying to follow a routine.

The advantages of an InSinkErator hot tap are endless, from grabbing a very quick cup of coffee to start the morning off to being able to enjoy a cup of tea later on in the day without waiting for the kettle to boil.

A hot tap is also invaluable when you want instant hot water to quickly make dinner later on particularly when you’re tired and need quick and easy food preparation. When you start weaning, hot taps are excellent for loosening the skin on fruit and vegetables making them far easier to peel before pureeing ready for your baby to enjoy.



Safe Enough for Inquisitive Hands


Many new mums worry about the safety of hot water taps but actually, the InSinkErator models are perfectly safe because they are all fitted with a safety switch or mechanism so there’s no chance of a young child scalding themselves.

Also, it’s worth mentioning that hot taps can be positioned on the worktop alongside a regular tap so they are set back from very little, nosy hands. For your convenience, there are various tap style options too. For example, there are separate hot taps that sit alongside your regular taps, or there is the complete 3 in 1 tap which features a normal set of taps along with a hot tap.



Safe Enough for Inquisitive Hands


Saving Valuable Time


Hot taps are excellent for adding water to a washing up bowl and they’re superb time-saving devices. If the average kettle takes 4 minutes to boil up and you enjoy five cups of tea or coffee a day that’s twenty minutes wasted just waiting for a kettle to boil! Hot taps mean no waiting, no time-wasted. Think what you could do with that extra twenty minutes every day; hang out the washing, sterilise your bottles, bath your baby, indulge in a nap…the list is endless.


Hygienic Food Waste Removal


So, a hot tap is a definite must-have in a new mother’s kitchen and the benefits of having a hot tap will last for the life of your kitchen too but there’s another excellent kitchen appliance designed to make your life so much easier and that’s the InSinkErator Waste Disposer.

Having a food waste disposer means you can get rid of food waste in an instant, just by flicking a switch and running cold water. When your baby is old enough to enjoy those first food flavours you’ll find your food waste increasing because there will be lots of scraps from peelings, cores and unused food. Rather than put it in your food brown bin, a waste disposer is a quicker, cleaner and far more hygienic method.


​​​​​​​

Hygienic Food Waste Removal


Better Family Health


Remember, food waste can stay in your brown bin for up to a week and there are really not many things more unpleasant than opening it up to deposit more food waste in it when there is already a mountain of rotten food in there.

The rotten food develops bacteria quickly, attracts pests (especially in warm weather) and the smell in grossly unbearable! Bacteria itself poses a health hazard and when you’ve got a young family you definitely don’t want to put anyone’s health at risk particularly when your baby starts to explore – who wants a brown bin emptied all over the kitchen?



family-time


Safe to Use


An InSinkErator food waste disposer means there is no odour, no food waste and it’s so quick and easy to use plus with today’s almost silent versions, you won’t disturb any of the family, especially a peacefully-sleeping baby.


InSinkErator Waste Disposers use a grinding mechanism which pounds food against the side reducing it to tiny particles before it travels away from your pipes, so there’s no chance of danger when using them.

Buy online and we'll install it for you


If you don’t want the hassle of installing your tap by yourself, we are here to help. Take advantage of our complete installation service. Our installation agents will come to you and install your new tap in a timely manner - you won’t have to lift a finger!



Please enable JavaScript to use this website.