Why You Need Instant Hot Water Tap
From making delicious hot drinks in an instant to speeding up countless kitchen tasks. Once you have an instant hot water tap you'll wonder how you ever coped without it.
In the past few years hot taps have become one of the must-have kitchen appliances.
They’re possibly the most useful addition to any kitchen because of their convenience and serviceability plus they save valuable time which is so important especially living in an age when everyone expects instant results.
Whether you’re thinking of adding one to your existing kitchen or you’re toying with the idea of including one in your new kitchen, there are so many advantages to choosing a sleek, smart, state-of-the-art InSinkErator model.
As with any modern appliance, you’d expect a hot water tap to look great and gain many admiring glances.
The InSinkErator models certainly do!
There are various options available from the InSinkErator hot tap collection and what you’ll notice about our hot taps is that they resemble regular taps very much.
They can be a combination of both regular hot/cold and the boiling tap such as the InSinkErator Combined Main Tap 3N1 which ticks all the boxes for a modern, sophisticated kitchen tap
InSinkErator hot taps are displaying a variety of finishes and blend perfectly with today’s modern style kitchens but equally can be fitted to traditional settings just as well.
As an example, if you want to fit one to your existing tap configuration, the H3300 Steaming Hot Water Tap is just one of the fantastic choices available from InSinkErator.
InSinkErator hot water taps have a 2.5 litre capacity in their tank and inside the tank there is a heating element which boils up the water to a very high temperature (approximately 98C).
Using any of the InSinkErator models is easy.
When you pull the lever, the hot water comes through the tap just like a regular tap – except it is boiling hot and there’s no waiting for it to heat up.
Additionally, our hot taps come with a filter inside which keeps the water nice and fresh, removing impurities before it reaches your cup or your saucepan.
A hot water tap gives you flexibility because it delivers boiling hot water, in an instant.
There’s no need to wait for your kettle to boil and when you’ve got no time to spare, that cup of tea must be delivered – fast!
Hot drinks have always been immensely popular no matter what time of the day and when it’s a cold day instant hot water is a godsend!
Then of course, who doesn’t love a mid-morning cup of tea or coffee with a favourite biscuit and who can resist a hot drink at night before bed?
Waiting for the kettle to boil can seem like a laborious task so having a hot water tap to hand is a fantastic time-saver.
It’s also well worth mentioning that hot water taps don’t just deliver boiling water for tea, coffee or other hot drinks, they are a fabulous cooking aid.
As an example, they produce instant hot water when you’re cooking vegetables on the HOB and when you need to get a pan of boiling water going for pasta.
They’re also excellent when you want to boil an egg, no more waiting for that pan to start bubbling and when you’ve got a tricky jar to open, just loosen it using instant boiling hot water!
For concerned parents of young children, rest-assured that they are completely safe because every single InSinkErator model comes with a safety feature so there’s no risk of accidents.
You can easily add one to an existing kitchen or if you want to replace your existing tap system you could purchase an all-in-one set of taps to include a hot water fitting.
The main fitting stays out of sight, with a thermal tank that lives inside your kitchen cupboard underneath your sink.
This is where the hot water is housed so when you turn your hot water tap on, boiling water appears within a split second.
Hot water taps are well worth the extra investment because in the long term there are money saving opportunities.
A kettle’s boiling time takes time and this uses up costly electricity.
Remember, it’s rare that anyone would run out of hot water from a hot water tap but if it did happen, it takes as little as ten minutes to re-heat to capacity and once hot, because of the insulation technology the water stays hot!
Don’t waste anymore of time boiling up kettles, we know from a report from The Energy Saving Trust that the Brits waste £68 million per year on
electricity just boiling kettles. 75% of those kettle-boiling people only use a fraction of the water for hot drinks!
It takes on average 4 minutes to boil 1 litre of water in a kettle.
If someone drinks 25 cups of tea a week and boils the kettle each time that’s 1 hour and 40 minutes just waiting for it to boil!
Save money for something else and use the time it takes to boil a kettle to do something more pleasurable, such as choosing a favourite biscuit to enjoy with an (almost) instant cup of tea!
If you don’t want the hassle of installing your tap by yourself, we are here to help. Take advantage of our complete installation service. Our installation agents will come to you and install your new tap in a timely manner - you won’t have to lift a finger!
Want to speak to a member of our team? We’re here to help