Garbage Disposal Myths
Do you think that garbage disposals harm the sewer system? Have you heard you can’t use a garbage disposal with a septic system? Get the facts on garbage disposals from the company that invented them.
A garbage disposal grinds food waste to easily flow through a home's plumbing and into a septic tank. Once there, food scraps decompose faster than other waste sent into the tank. Because food scraps are 75% to 90% water, they add very little to the solids that settle at the bottom of the tank. Studies show that septic systems attached to a garbage disposal don't require more frequent pumping than those that aren't.[1]
[1] Study of food waste degradation in a simulated septic tank - Hongjian Lin, Yuchuan Wang, Leif van Lierop, Carlos Zamalloa, Casey Furlong, Michael Keleman, Bo Hu, 2019
Want to know how you can reduce the negative impact of food waste on the environment?
Want to know how you can reduce the negative impact of food waste on the environment?
Learn More about How InSinkErator Garbage Disposals Can Better Support Your Septic System.